Prestigious Middle East project for Prysmian
Dubai (United Arab Emirates). The
new
Emirates Airlines
Headquarters has been provided with Prysmian’s fire performance cables.
Over
300km of cables, FP200 Flex and FP400, were supplied for being used in the fire
alarm systems in the
airline’s modernized impressive nine-storey building, which has two basements and
a tunnel leading staff underground directly into the airport.
Prysmian strong presence in the Middle East made the company’s fire performance cables the
obvious choice for the project.
Prysmian cables have been chosen for many prestigious developments in both Dubai and Abu
Dhabi: to mention a few, fire resistant cables are at the very heart of the most
spectacular and complex developments, like
Burj
Dubai, the world’s tallest building ever constructed.
As Antony Vas, purchasing manager for International Electromechanical Services (the company
that installed FP cables in the Emirates Airlines Headquarters) confirms
“buying cables from a
reputable manufacturer and distributor is one of the most important deciding
factors when purchasing cables.” Reliable cables for all fire alarm and emergency
systems was absolutely necessary for the development, which took two years to complete. This,
however, was not the only reason for choosing Prysmian. Vas also commented on the cables’ ease of
use,
“the cable was very easy to install and of very good quality” he said.
Related Products:
FP
Plus
FP200
Gold
FP400
Related News and Informations:
Prysmian at home
in Ikea Southampton
Prysmian
serves up fire protection at Wimbledon
Prysmian tackles fire performance
at Twickenham Stadium
Royal Festival Hall re-opens with
symphony in fire safety
Prysmian Powers
Welsh Athletics
Prysmian protects
Portsmouth’s patients
The sky’s the
limit
Fire
Middle East Magazine - Are you getting the performance you expect?
Archivio
Highlights
|