Glossario  |  Contatti |  English  |  Cerca nel sito

  
Il Gruppo Prysmian
Soluzioni per il tuo Business
Investor Relations
Lavora con Noi
Comunicazione e Media
The Neptune Interconnection

Now in service the new high-voltage transmission link between New Jersey and Long Island, New York.
At the end of June 2007, and one month ahead of schedule, Prysmian handed over the Neptune, a new high-voltage direct-current (HVDC) transmission link between Sayreville, New Jersey, and Long Island, New York.
   • Neptune's technology

   • Read the press release
After a successful trial period the Neptune interconnection is now in service, just in time to face the summer period. The Neptune cable system provides Long Island with the opportunity to significantly diversify its energy resource options with the possibility of purchasing power from one of the most diverse and competitively-priced power transmission organization in the United States, called "PJM", which controls electricity flows in all or parts of Delaware, Illinois, Indiana, Kentucky, Maryland, Michigan, New Jersey, North Carolina, Ohio, Pennsylvania, Tennessee, Virginia, West Virginia and the District of Columbia and contains more than 100,000 MW of diversified and relatively low-cost power generation.
That's why, thanks to the Neptune, LIPA (Long Island Power Authority) is now able to acquire lower cost energy on time for the peak summer season, when the demand for electricity is higher, thus meeting the needs of about 600,000 average-sized homes in a cost-effective and sustainable way.
The Neptune Regional Transmission System consists of a 65 mile electric transmission line from Sayreville, New Jersey to Nassau County on Long Island via undersea and underground cables.
The project included the manufacturing, transport, installation and commissioning of a 660-MW (500 kV) High Voltage Direct Current (HVDC) submarine turn-key cable system that interconnects power generation resources in New Jersey to electricity consumers in Long Island, along a distance of 65 miles (more than 100 km). The largest portion of the route – more than 50 miles - runs underwater across the Atlantic Ocean out of the New York Harbor area; 14 miles run underground (either direct buried or in conduit) in the existing right-of-way of the Wantagh State Parkway.
Prysmian Power Cables and Systems USA LLC, in consortium with Siemens Power Transmission and Distribution Inc. USA, provided the engineering, procurement, and construction services for manufacturing and installation of the cable, construction of the converter stations and installation of station components.
Mappa del Sito  |  Informazioni Legali  |  Copyright © 2007 All rights reserved. P.I 04866320965